This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2982: IO(PK) Peak output current

Part Number: LP2982

Hi support team,

MIN is greater than TYP.


Isn't MIN=100mA and TYP=150mA for both A and non-A products?

Regards,
Dice-K

  • Hi Dice-K,

    Yes, that is clearly a datasheet error and I will place it in the correction log to be fixed.

    Also yes, as you've pointed out I think there was an issue when the datasheets were copied over as the formatting didn't align exactly so the automated system made an error. I will submit this as a change, and let you know if I hear back and it is truly different typical, but at this point I will be submitting a change request.

    Regards,

    John