Part Number: LM5110
Hello,
What is the maximum rating for the OUT_A and OUT_B pins of the LM5110-2?
Please tell me the MIN and MAX. There is no description in the data sheet.
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5110
Hello,
What is the maximum rating for the OUT_A and OUT_B pins of the LM5110-2?
Please tell me the MIN and MAX. There is no description in the data sheet.
Best regards,
Hi Kaji,
Thank you for reaching out! Our expert on this device is currently out of office because of US holiday, and we'll get back to you when we're back in office.
Vivian
Hey Kaji,
Thank you for your question!
For the LM5110 output pins, in the Pin Functions table in section 6 of the datasheet calls out OUT_A and OUT_B as capable of sourcing 3A and sinking 5A of current as well as the voltage swing of the output being from Vcc to Vee. The recommended operating condition of Vcc to Vee is 3.5V minimum to 14V maximum.
Let me know if you have any further questions.
Thank you,
William Moore
Thank you for your reply.
I understand the recommended operating conditions.
Then, is it correct to think that the absolute maximum rating is MIN=-0.3V and MAX is 15V?
Best regards,
Hey Kaji,
Yes, the absolute maximum ratings for Vcc to Vee is -0.3V to 15V. So, the absolute maximum ratings on OUT_A and OUT_B would be the same.
Let me know if you have any further questions.
Thank you,
William Moore