Hello Team,
in order to enable the part at the desired voltage my customer needs to know the internal pull down resistor value, please. If possible can you provide R over Vin and temperature, please?
|
Parameter |
Description |
Test conditions |
MIN |
TYP |
MAX |
UNIT |
|
REN_PD |
Smart-Enable Internal Pulldown Resistor |
VIN = 3 V to 17 V TJ = –40°C to +150°C EN = LOW |
|
|
|
MΩ |
Thank you and Best Regards, Hans