Other Parts Discussed in Thread: BQ24308
Hi,
We are using the BQ24314 P.N in our application as an overload and an over voltage protection circuit, see below.
The OUT pin supplies voltage to an electrical circuit with an approximated equivalent of 150uF total capacitance (the limit current is configured for 285mA).
The on/off operation is made using a slide switch (which has a bouncing effect while closed).
The BQ24314 works properly most of the time, but occasionally gets into a protection mode (completely shuts down until we disconnect and connect the input supply back again).
The output current measurement made during the shutdown showed that the OCP condition (15 cycles according to the datasheet) do not happen at all.
Only a single current limiting period (marked in purple) was captured.
Note: the input voltage is stable, with a 1V drop (from 5V to 4V) so no input overvoltage happens.
A question please - Is there any errata sheet describing this phenomenon? Did anyone encounter a similar phenomenon with this chip?
BR,
Yoav