Other Parts Discussed in Thread: WEBENCH-CIRCUIT-DESIGNER
Dear Specialists,
My customer is considering TPS43060 and has a question.
I would be grateful if you could advise.
---
I have a question about the result between WEBENCH and Calculation Tool(SLVC471)
I ran a simulation with WEBENCH from TPS43060 Product Folder under the following conditions, but the design could not be created.
When using WEBENCH-CIRCUIT-DESIGNER, simulation results were obtained using an ideal FET. In some cases, this result could not be obtained.
22_26Vin 34Vout 15.3Aout WBDesign142.pdf
What is the cause?
TPS43060
Input: DC 22V - 24V
Output: 30V at 16A
Temperature: 30°C
On the other hand, we were able to obtain calculation results using the Calculation Tool (SLVC471).
TPS43060 24Vin 34Vout15.3Aoutput.xls
Is this result feasible?
---
I appreciate your great help in advance.
Best regards,
Shinichi