This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75453B: Does it have an internal pull-up resistor on each input pin?

Part Number: SN75453B
Other Parts Discussed in Thread: SN75451B

Hello,

My customer works on SN75453BD with VCC=5V and connected pull-down resistor(22kOhm) on each input pin to expect low level on the output.  However the output was Hi with the input pin voltage level of around 1.5V.  Would you please tell me the reason why it is?  Does it have an internal pull-up resistor on each pin even though the datasheet doesn't show such information?  I don't think it would, but does it have dependency on package?

Best regards,

Yoshikazu Kawasaki