This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM337:LM337KVURG3

Part Number: LM337

お世話になります。

LM3KVURG3を使用して-5V入力から-337.3Vを出力できるか確認してください。

どうぞよろしくお願いいたします。

  • Hi Fukushima,

    This is regarding LM337KVURG3 being used to output -3.3V from -5.0V input.

    For rated performance of the device Vin-Vout = –3 V to –40 V. 

    Since here Vin-Vout= -1.7V, device will work but will be in dropout or close to it. So it may not be able to provide the maximum rated current for the device.

    Thanks,

    Bobby