This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS748A: How to calculate Soft-start-time

Part Number: TPS748A


Hi,Team

Please tell me how to calculate soft-start-time.
There is a soft start time calculation formula in 8.2.2 Detailed Design Procedure in the data sheet below.
I believe the formula for calculating tss is as follows.

tss = (Vss×Css)/Iss

We also confirmed the contents of 6.5 Electrical Characteristics below.
Iss was 7.5[uA] when Vss=0.4[V], and Tss (Soft-start-time) was 1.2[ms] when Css=10[nF].
And I calculated it using the above formula.

tss = (Vss×Css)/Iss = (0.4[V]×10[nF])/7.5[uA] = 0.5333[ms?]

However, the calculation result was not tss = 1.2[ms].
Please tell me how to calculate Soft-start-time.

Best Regard

  • Hi,

    The datasheet lists the voltage where Iss is measured, but Iss will be almost constant across Vss voltage.

    You can use the same equation you pointed out to calculate soft start time.

    But Vss is not mentioned with the equation. You can calculate it using tss = 1.2 ms, Css = 10 nF, Iss = 7.5 uA giving Vss = 0.9 V

    Regards,

    Bobby