Part Number: TLC5926
Other Parts Discussed in Thread: SN74HC595, TLC59283
Hi,
I would like to use TLC5926 or similar part to turn on a group of LEDs in a sequential way (meaning turn on first LED for 100us, then turn it off and then at the same time turn on second LED for 100us, then turn it off and then at the same time turn on third LED for 100us, .... and so on).

My questions are:
(1) Can TLC5926 do this?
(2) If so, how should I set all input signals? LE always high? OE always low? And can I daisy chain multiple TLC5926 (SDO -> next SDI) to drive more than 16 LEDs?
(3) If not, could you recommend other components to implement this function? (The reason I prefer to use LED driver IC is that I can have constant current driving, rather than using shifter register IC for constant voltage driving).
Thank you.
Jonathan