Other Parts Discussed in Thread: ISO5852S
I am using ISO5452 driver in solar inverter (three phase) with DC bus ranging from 200V to 800V with switching frequency 4kHz. I bought ISO5852 instead of ISO5452 due to component non-availability. Most of the key specifications matched for both devices. However I'm facing issues when I have 4x ISO5452 and 2x ISO5852 drivers in my inverter. The de-sat current limiting resistor is burning/fail open where ISO5852 devices are present. Any suggestion/recommendation to address this issue?