This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC23513: Comparison of UCC23513 and NSI6801

Part Number: UCC23513
Other Parts Discussed in Thread: TLV9004,

Hi team,

My name is Sophia, TSA cover SOLAX, who is a top leading energy storage inverter customer.

Recently, we found a new project of 3phase hybrid inverter, and get a gate driver UCC23513 to replace their solution NSI6801. We promoted TLV9004 to compete.

Could you please give me a comparison of UCC23513 and NSI6801?  

Thanks

Best Regards

Sophia Zhang

  • Hi Sophia,

    Here is a comparison chart my team put together for this competitor device:

    PARAMETER

    Novosense

    NSi6801B

    TI

    UCC23513BDWYR

    TI System Benefits

    Isolation Technology 

    Capacitive

    Capacitive

    Isolation Rating

    Reinforced

    Reinforced

      Isolation

     CMTI (min)

    150kV/us

    150kV/us

     VIOWM: Max Working (DC)

    2121V

    1500V

     VIOTM: Max Transient

    8000V

    8000V

     VISO (rms, 60s): Max Surge

    5700V

    5700V

      Output Driver

     Max Drive Current

    +5 A / -5A

    +4.5A / -5.3A

    Sink having a higher magnitude allows for safer turn-off

     Max Differential Voltage

     (VDD-VEE)

    35V

    35V

     Driver Specs

     Prop Delay (max)

    100 ns

    105 ns

    Faster communication between pieces

     Part-to-part Delay Matching (max)

    35 ns

    25 ns

    PWD: Pulse width distortion

    30 ns

    35 ns

    Power-up delay (max)

    N/A

    30 us

     Tj_Max

    150°C

    150°C

      Package

     RθJA

    125°C/W

    126°C/W

     Package Options

    SOIC-6 WB

    4.68mm x 11.5mm

    Stretched S-O6

    4.68mm x 11.5mm

    Best regards,

    Sean