This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS568215: Inquiries about TPS568215RNNR

Guru 11480 points
Part Number: TPS568215


Hello,

My customer is using the TPS568215RNNR with VIN=13V and VOUT=1.509V.

They have some questions about the device.

Q1) Is there a shutdown function according to input voltage changes? If so, what is the input voltage for shutdown under the above user conditions?

Q2) What is the current in the internal diode?

Q3) How many voltage output modes can the user select from this device?

Thank you.

JH

  • Hi JH,

    1. As long as input voltage is in the range 4.5V-17V. Vin won't shutdown. Vin=13V, Vout=1.509V, No Vin shutdown.

    2. What do you mean the current in the internal diode? What is internal diode?

    3. Please refer to table 5 in the datasheet for inductor/output capacitor/switching frequency selection. Then based on table3 to select MODE pin setting.

    Hope this helps,

    Thanks,

    Nancy