Part Number: TPS717-Q1
Other Parts Discussed in Thread: TPS717
Hello,
My customer is using the TPS71733QDRVRQ1 with VIN=5.5V and VOUT=3.3V.
They have some questions about the device.
Q1) Is there a shutdown function according to input voltage changes? If so, what is the input voltage for shutdown under the above user conditions?
Q2) What is the current in the internal diode?
Q3) How many voltage output modes can the user select from this device?
Thank you.