Other Parts Discussed in Thread: TPS62816-Q1
According to the datasheet, this device can operate with and input voltage as low as Vin= Vout + Iload*Rdp. This would mean that for a design outputing 3.3V @ 0.5A, it would works with an input voltage as low as 3.32V aprox. My concern is that the online workbench tool does not allow to set the input voltage below 4V. Is there another limitation that perhaps I didn't catches from the dataseet?
On the other hand, is there available a spice model that can be loaded into TINA?
Cheers,
Javier