Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563202: schematic review

Part Number: TPS563202

Hi expert 

could you please help review this schematic, because we don't have suitable 1.2uH or 1.5uH inductor, we used 2.2uH. Input is 12V, output is 0.8V~1V,2.4A

  • Hi Feeney,

    Thanks for reaching out! Please see my comments below:

    1. Please ask customer to follow recommended component values table in ds: inductor changes to 1.2uH, FB networks change to recommend value and add one more 22uF Cout

    2. What is the function of VDD_EE_PWM signal? Does customer want to use it to change Vout? 

    BRs

    Zixu