This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS737: PS73701DCQR的dropout电压和VOUT(nom)

Part Number: TPS737

1.200mA负载不是对应dropout几十mV吗?最大值也按照500mV考虑?2.VOUT(nom)是个定值2.5还是我需要的电压

  • 李立松先生,您好!

    我附上了关于Iout和Vdo的资料。 在200 mA时,约为25 mV。 当Iout = 1A时,最大VDO为500mV。 我还附上了一个公式,您可以根据反馈电阻器来确定输出电压。 我希望这能帮助你。

    如果您有任何其他问题,请告诉我。