Other Parts Discussed in Thread: TPS3808, ISO1641, TPL5110
Hello,
I'm working on schematic for 8 cell battery voltage monitor, based on BQ7694202. Since all other features are not needed, they are disabled in a way that unused pins are connected to Vss or left floating as proposed in the table 16-3 in a datasheet.
I just would like ask for a schematic check. Schematic is available here: https://we.tl/t-2V8v50NjM8
I'm not sure if I implemented wake-up circuit in a proper way. Idea is to change BQ7694202 state from SHUTDOWN to NORMAL approx. 2 seconds (with TPS3808 IC) after battery balancer connector is connected to CN20 connector. In a such way pin TS2 is pulled down indefinitely, but I'm not sure if this is acceptable or should be pin released after some time (after device state switched to NORMAL state)? On the other side, state change from NORMAL to shutdown is guaranted when battery balancer is removed from CN20 connector. Is resistor R41 necessary or could be omitted since internal pull-up resistor is integrated in IC on TS2 pin?
What do you think about balancer resistor and balancer capacitor values (100R and 1u) since they are on the max. proposed side? Do you suggest to use lower values?
Somewhere I read that BAT and CP1 pins could be connected together if DSG and CHG pins are not used. Is this right?
Is resistor R26 needed between PACK pin and top battery cell?
Any other suggestions are welcome!
Many thanks,
Kind regards,
Dejan.