Other Parts Discussed in Thread: CSD18532Q5B
I saw that the FET above is listed as a logic-level FET @ TI.
It has a typical gate threshold voltage of 2.8V and a max. of 3.4V.
Just wondering: Is there an (more or less) industry-agreed criterion what constitutes a logic-level FET?
Some go up to 4.5V, but TI's filter apparently not.
My personal opinion: Vgsth should be 2V or lower so that at venerable TTL-high(min) of 2.4V it is clearly turned on.
Actually that would have to be the threshold maximum.
I think we can agree that then it is a logic-FET for sure, even if some logic families nowadays may have lower supply voltages.
But marketing guys may well disagree with me, so - being an engineer - I'd prefer to have a hard rule.
There must have been a time when this term first came about. Was it with HC or with CD4000...? I do not know.
Just wondering how TI does it officially.