Please allow me to confirm the usage of TPS54231.
While using the TPS54231 as an inverting power supply, the same peripheral component failure has occurred on multiple boards.
The design of the power supply circuit is based on the following.
www.ti.com/.../slva317b.pdf
The points we would like to check are as follows.
Is it OK to use the inverting power supply of TPS54231 as a power supply for both power supplies?
Should we use the EN pin, which is currently open?
Also, how should I use the EN pin when using it as an inverting power supply?