Other Parts Discussed in Thread: TPS7A26, TLV767
Hi team,
I have two questions on the application of TL5209. In the datasheet, it points out that the ESR of output CAP should not approximately equal to 1 ohm on page 14.
Question 1:
I’m not sure if the cap at the end of the load is included in the output cap. Or does it just mean the ESR of Cout?
Question 2:
The datasheet just states that ESR cannot be equal to 1 ohm. Are there any other constraints on ESR? For example, max and min values?
Why can't ESR be 1 ohm in this case, and what is the value range of ESR related to?
By the way, the TL5209 seems to be a very old device, do you have a recommendation for a more suitable replaceable device?
Thanks for your support.
Comi