This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS631010: TPS631010YBGR

Part Number: TPS631010

Hi,

I am using TPS631010YBGR for generating a 3.3V at 1A output. Please review the schematics and dro[p your valuable comments.

Details:

Input Voltage: 2.8-4.2V

Output Voltage: 3.3V

Output Current: 1A

Components:

C4 decaps: 22uF, 10V

C6 decaps: 10uF, 10V

L1: 1uH, 4.1A

C20, C25 decaps: 22uF, 10V

C26 decaps: 10uF, 10V

Schematics: