Hi, I'm using [LM61480Q5RPHRQ1, VoutFIX = 5V, Iout = 8A]. I see this in the layout guideline "Make the top and bottom PCB layers with two-ounce copper and no less than one ounce.".
I'm using 6-layers PCB which every layers are 1oz. thickness. Will any problem occurs If the top layer is not 2oz. Can another layer be used to add more copper? (especially SW-node, add more coppers to this node using vias to another layer good idea or not?).
Layer 2, 5 is GND plane. The left spaces will be poured with GND Vias later.
Ps. If there're any bad design I may not realise, please tell me.