This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5008: minimum output voltage ripple

Part Number: LM5008

Datasheet: "A minimum of 25 mV to 50 mV of ripple voltage at the feedback pin (FB) is required for the LM5008."

What happened is that the design is modified. The 1 Ohm resistor in series with the output capacitor (tantalum) is replaced by a 0 ohm resistor. The ESR is now (to?) low, causing the ripple on the FB pin to be about 10mV instead the required 25mV min. But... The converter seems to work fine, there is no instability and also with a step response from 50mA to 300mA there is no stability issue. 

I have two questions:

1. what is the real minimum ripple voltage at the FB pin?

2. what happens when the ripple is to low with a converter using the hysteretic control scheme? Now, it is not unstable, the max output current current is possible and the converter is not heating up more than expected. Also the switch node looks fine during constant load and step load, there are no extra pulses as mentioned in AN-1481 Figure 3.

Why is the converter working?