This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138064AEVM149: Power management forum

Part Number: UCD3138064AEVM149
Other Parts Discussed in Thread: UCD3138, UCD3138A

Hello experts, I am currently using UCD3138ALLCEVM-150,During the debugging process of LLC, if I want to obtain a PWM wave with asymmetric dead time, should I only need to adjust the following part?

  • Can UCD3138 generate asymmetric PWM in resonant mode? In other words, make DT2 not equal to DT1+DT3

    Because my driver chip may have delays, resulting in inconsistent dead zones between the upper and lower driver waves of the half bridge,so I want the dead zone between 0A off and 0B on to be unequal to the dead zone between 0B off and 0A on
  • Hello,

    The deadtime configuration between UCD3138 and UCD3138A. If you use UCD3138, the answer is yes.  You can use EV1.2.3.4 to get asymmetric deadtime.

    UCD3138A offers symmetric deadtime.

    Regards,