This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alex,
Thank you for using E2E forums, I will answer you next week.
Thank you for your patience.
BR,
Haroon
Hi Alex,
Thank you for using E2E forums, the first two pictures are top view and then the third is the bottom view hence you have that rotation or flip of the pin configuration.
BR,
Haroon
Hi Haroon,
unfortunately, it still doesn't add up. I agree that the third picture is the bottom view. If you flip it upside down, pin 1 would be on the bottom left corner. The pin 1 indicator would also be on the bottom left corner, and the thermal pad is still vertical. You now rotate the IC 90 degrees clockwise in order to have the chip in the same rotation as in pictures 1 and 2.
So after rotation, pin 1 is now on the left top corner (where pin 16 is shown in the third picture). But the thermal pad also rotates 90degrees, hence the thermal is now horizontal and not vertical anymore. And this is where there will be a mismatch with picture 2.
TL;DR:
The thermal pad in your datasheet does not match the actual chip.
Please have a look at it based on my above description. Do you agree with my confusion?
Thank you,
Hi Alex,
Oh ok you mean the thermal pad's orientation? let me have a look at the IC and come back to you.
Please expect a response next week, due to my narrow bandwidth and also national holidays this week in Germany.
Thank you for your understanding.
BR,
Haroon
Hello Alex,
Sorry for the delay, I ordered some components and it seems that we need to update the datasheet. I hope to be able to come back with a definitive answer in a few days. I want to make sure that I am not overlooking anything.
Best regards,
Brigitte
Hello Alex,
The layout drawing is showing the thermal pad in the wrong orientation, as you already found out. With the next datasheet update we will update this drawing as well. The package drawings at the end of the datasheet give the exact information as this is our reference for production.
Best regards,
Brigitte