Part Number: LM3485
Other Parts Discussed in Thread: LM3489EVAL
你好!
1.The input voltage is 24V, and the output voltage is 3.6V;


2.Please help confirm the impact of the size of the inductance on the output voltage. We have used two brands of inductors in use, one with a measured inductance value of 43uH and the other with a measured inductance value of 47uH. The result is that the voltage at 43uH is close to 3.6V, while the voltage at 47uH is close to 3.72V.