Hello,
It is written in the datasheet that FLT will not reset until VOUTx has risen to VVS – 1.8 V.
We are keeping output shorted with a wire all the time and behavior is such that device goes in and out from fault periodically. At the beginning device shows fault state normally. After it starts with "non fault" state, by percentage, device is much longer in fault state - lets say 80/20%.
But as more and more milliseconds pass, this relation is becoming 40/60% in "non fault" state favor.
Device is kept in auto-retry mode all the time.
This is something related to thermal shutdown obviously, I'm just not sure why it shows that all is fine when obviously it is not. Vout has no chance to reach voltage that will reset Fault signal as it is short wired.
Best regards,
Miroslav