Other Parts Discussed in Thread: TPS62903-Q1,
Hello TI Team,
We are using TPS62130AQRGTRQ1 in our design and having following observations:
1. We are having an application of converting the 5V input to 3.3V output. The inductor value used in design is 1uH and the output capacitor used is approx 57uF. When we are loading the buck regulator with electronic load the output voltage and the efficiency of the buck reduces drastically if the output current is greater than 2A. Below are the readings from the testing:

Even after removing the efficiency of inductor, the power dissipation at 2.8A for the IC is 1.4W. We have also observed the delta of 30 degree self heating from the ambient temperature. Can you please let us know how to improve the efficiency of the buck or request you to suggest the alternate part number with the same footprint package.
2. The TPS62130AQRGTRQ1 is rated for 125degC operating temperature. However, in the datasheet it is mentioned under the recommended operating temperature that Tj value of the component should not go beyond 125degC. Can you please let us know how the ambient temperature and Junction temperature values are same?
3. In the absolute maximum ratings it is mentioned that Tj value can go upto 150degC but it will impact on the reliability of the component based on the note mentioned in the datasheet. Can you please let us know the limits for the Junction temperature with which the lifetime of the device is not getting impacted?
Your immediate response on these questions will be highly appreciated.
Regards,
Khemraj Suthar