There seems to be an error on the LMZ34002EVM schematic shown on page 7 (Figure 2) of the EVM datasheet. The schematic shows the CLK pin 31 connected R8 (the other side of R8 is connected to A_VOUT). It also shows the RT pin 30 is floating. In fact, it should be the opposite: RT pin 30 should be connected to R8 and CLK pin 31 should be floating.
The example layout (page 9, Figure 5. Layer 1) shows the correct wiring, however, the schematic is incorrect.
Flip Sarrow