LMR51430 support,
I went through the equations in section 9.2.2.4 of the datasheet, and the value for the inductor selection is different from the result given in the datasheet. It looks like the calculation is based on a Vin Max of 12 V rather than 36 V, even though it should be 36 V according to the Design Example Parameters.
Please let me know the correct way to handle this calculation.
Thanks,
Darren