Hi there,
Running Parameters: Vin = 20V, Vout = 13.85V, Iout = 32A, L = 18uH, Cout = 3mH, Cin = 8mH, Rcs = 1.5mOhm.
We are having an issue with the output voltage rail collapsing after running for 15 to 30 minutes at rated full continuous load.
Can we talk directly so I can show images?
Cheers