Part Number: TPS7A4501-SP
Other Parts Discussed in Thread: PSPICE-FOR-TI
Hello,
We are running simulations with the phase and gain analysis of the TPS7A4501-SP, and when we try to simulate the circuit that is in the SEE report, it is inherently unstable with a crossover frequency in the MHz range and a phase <10 degrees. It seems like removing the FF cap (470pF) makes it stable, but we just want to confirm whether or not we are using the correct simulation file, or if there is an issue with the simulation file as we are following the circuit in the SEE report.
Our current simulation parameters are as follows
1. VIN = 15V
2. VOUT = 12V
3. Output capacitance, 22uF, 1uF, 100nF.
4. Input capacitance is 15uF.
5. Feed forward cap 470pF
6. PSpice simulation file: worst case analysis.
We are running the simulation on LTSpice, so Im not sure if that might cause an issue as well.
Thank you
Albert