Other Parts Discussed in Thread: TPSM82913
Hello,
The TPSM82912 input voltage range is 3 to 17V. Would you have efficiency curves for Vin=3.3V with outpout voltage 0.8V, 1.2V and 1.8V?
regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Will check and try to give feedback tomorrow.
BTW, what's your application?
Yuchang
Hi Amaud
Got it, Yuchang are working on it and will give the feedback later, thanks!
Here are 1MHz efficiency with TPSM82913, which can be referred for 82912.
No second filter
up to down is 1.8V/1.2V/0.8V
Yuchang