Unfortunately we are facing severe problems with the TPSM82821 (LiPo to 3.3V) voltage regulator one of our boards - a detailed summary is attached.
1. The regulator shows a dramatically increased current draw, at capacitive loads, that are within the datasheet limits.
When loaded with a nominal (derated) output capactiance of 40-45µF, the regulator will draw short high current spikes (>=30mA) without any load. This increases the average quiescent current dramatically.
The output seems to be stable in this condition, while the input current consumption increases.
2. The regulator shows an increased current consumption in low-dropout mode.
While the datasheet states 10µA maximum quiescent current, the quiescent current increase to the 100µA+ range.
The behaviour of (1) and (2) seem to be independent of each other and both effects seem to very between device and device (but with a sample size of 2, this is really no metric at the moment).