This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23753: MDI interface maximum trace length

Part Number: TPS23753


Hello Team,

We are using TPS23753PW in our design for the POE 802.3af .
I have one concern , we are planning to place magnetics in one board and TPS23753PW in the different board which is main board and will connect the both board with FPC connector and cable . The Overall distance for the MDI signals(Tx_P, TX_N, RX_P, RX_N) from the magnetics to the Phy IC will be 200mm to 250mm . and also signal will travel through the FPC cables . Does this much distance between the magnetics and PHY IC are allowable ? will it create any issue ? will there be any signal distortion or the degradation?