before the device start, the 
output shart like RC curve, and when shut down EN pin, the output is still on about 300mV. could you explain why? and detail reason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
before the device start, the 
output shart like RC curve, and when shut down EN pin, the output is still on about 300mV. could you explain why? and detail reason
Hi Xiaodong,
Apologies for the late response.
Can you share the circuit diagram and waveforms as indicated below to better understand the issue? What is system load of 1V8 rail?
1. VIN and EN pin voltage, 1V8 voltage (Ch1), Inductor current (of Ch1)
Best regards,
Excel
hello Excel:
schematic as below:

waveform:


The power application is used head unit product and supply for serializer IC. input voltage is 3V3, EN pin is 3V3 from MCU.
Hi Xiaodong,
Thanks for the quick response.
There might be another source current (Isource = 300mV / 50ohm = 6mA) on 1V8 rail causing it not to fall ~0V when EN = Low. Can you isolate the 1V8 rail to any other connect and check the output voltage waveform again? Do you observe the same case in 1V0V rail?
Best regards,
Excel
Hi Excel,
you are right. after disconnect, the output is OK, this abnormal voltage is from load side.
thank you for your support!