Other Parts Discussed in Thread: BQ76940, BQ76952
Hello,
I want to control the charge and discharge of a 15S battery by connecting the BQ7694 integration behind the BQ25756 circuit.
I want to adjust the voltage according to the battery type and adjust the current when charging the battery cell connected in parallel.
I am thinking of using bq25756 for voltage and current adjustment.
I aim to use the bq7694 integration to receive battery data and use it on the monitor.
These two separate integrations will be connected to a tej MCU with I2C and the data will be controlled from there.
Can you give a block diagram about this?
I would also appreciate if you can share if there are alternative or auxiliary circuits that I should use.