Part Number: TPSF12C1QEVM
Other Parts Discussed in Thread: TPSF12C3QEVM,
Dear All,
I hope this message finds you well. I am writing to update you on our recent efforts involving the TPSF12C1QEVM and TPSF12C3QEVM active filters that we purchased to integrate with our single and three-phase passive filters. We have built various configuartions of the passive filter with a active filter such as 1-satge and 2-stage EMI filter with LC topology.
We successfully measured the attenuation of the combined filter (Active + Passive filter) using a vector network analyzer. In the common mode (CM) configuration, the active filter demonstrated excellent performance, providing an attenuation of about 20-28 dB in the frequency range from 100 kHz to 2 MHz.
However, when we conducted EMI measurements using the following setups:
LISN + Input filter (Active + Passive) + Inverter + 25m motor cable + Motor
LISN + Input filter (Active + Passive) + Switched mode power supply + Resistive load
We encountered challenges. Despite our best efforts, the active filter did not function as expected. We performed measurements both with and without the active filter, and the results were almost identical.
Considering this situation, I would greatly appreciate any suggestions or guidance you might have regarding our EMI measurement setup. Your expertise would be invaluable in helping us address these issues effectively.
Thank you for your time and assistance. I look forward to your valuable insights.
Best regards
Mohammad Ali