This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Request a power solution recommendation.

Hi

I need a solution that can satisfy the specifications below.

-spec-

Input: DC126~287V

Output: DC 350~600V (5KW)

Efficiency: Over 99%

Required condition: Non-isolated , bi-directional dc-dc 

Thanks