Other Parts Discussed in Thread: C2000WARE
Hi,
The TIDM-02013 ref design is for Single-phase 7.4KW.
I want to design a 15 kW single-phase system.
Is it possible to support us?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The TIDM-02013 ref design is for Single-phase 7.4KW.
I want to design a 15 kW single-phase system.
Is it possible to support us?
Hi Bosco,
May I know if your question is about requesting support for the 15 kw power converter design?
Thanks
Srikanth
Hi Srikanth,
Thanks for the reply.
I need similar design as TIDM-02013(Single-phase 7.4KW).
with specification, which can support 15KW.
Requirement:
Input= 230Vac
output= 400Vdc @ 15KW
Regards
Bosco
Hi Bosco,
You can refer to the TIDM-02013 code for Firmware development and can reach out to us for any additional support. It's available at C:\ti\c2000\C2000Ware_DigitalPower_SDK_4_04_00_00\solutions\tidm_02013. Mean while we will look at the possibilities to support your 15 kw hardware design.
Thanks
Srikanth
Hi Srikanth,
Thanks. Im going through it. Will reach out in case of any support.
Also pl., parallely guide on the hardware part.
Regards
Bosco
Hi, Bosco,
If you have a specific question on the design I can see what I can do to answer it. However, if you are looking for TI to assist in the hardware development of a full design, you will need to work with your local FAE to determine if this level of support is possible.
Thanks and best regards,
Brent
Hi Brent,
Thanks for your reply.
I just need the calculations to achieve my requirement(Input= 230Vac, output= 400Vdc @ 15KW) . In the present design TIDM-02013(Single-phase 7.4KW).
The rest I will take care
Thanks
Bosco
Hi, Bosco,
I don't have a generic calculator for a design like this.
If you need a detailed electrical design I'll need you to work through your local FAE to see if we can provide that level of support.
Thanks and best regards,
Brent