Other Parts Discussed in Thread: TL431, LM25037
Hello there,
I'm going to use LM25037 for controlling a half bridge converter and also an TL431 and optocoupler isolation for compensation circuit. Is it okay to implement the compensation using the TL431? Is there any reference available for designing the compensator circuit for the Half bridge converter using LM25037? The converter specifications are given below:
Vin- 54 to 73 V
Vout - 24V
Power out - 200W
Thank you