This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28781-Q1: Calculating VBUR target voltage VBUR_tgt

Part Number: UCC28781-Q1
Other Parts Discussed in Thread: UCC28781, UCC28782

Hello,

I am going through the design steps in the datasheet of UCC28781-Q1 to design a AC - DC converter. But I am stuck at VBUR calculations in 8.2.2.4 which says

"The procedure to determine the value of VCST(BUR) is quite complex and is not provided in this datasheet.
Instead, a soon-to-be-released UCC28781 Excel Calculator Tool automatically calculates this value based on
user input and determines the VBUR target voltage VBUR_tgt. Using this target value, it further determines the
appropriate values for RBUR2 and RBUR1 to meet the BUR pin targets based on user selections for the following
set of equations"

I am not able to find this excel calculator, could you please help me with this? I am not sure what value to use for VBUR_tgt.

Thanks in advance,