This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: TPS25750 +BQ25798

Part Number: TPS25750

Hi team ,

Kindly , Give Information how the TPS25750 will charge the battery if Non PD Adapter is connected?

  • Hello pooranessh,

    Without USB PD protocol, the TPS25750 should sink the maximum capability of the Non PD Adapter up to 15W (5V 3A) depending on the adapater's capability.

    5V/500 mA for USB2.0, 5V/900 mA for USB3.0, 5V/1.5-3A for USB Type-C. If BC1.2 is enabled the TPS25750 can sink up to 1.5 A from USB2.0/USB3.0. 

    Best Regards,

    Christian.