This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-02013: CLLC

Part Number: TIDM-02013

Hi,

The TIDM-02013 ref design is for Single-phase 7.4KW.

I want to design a 3 kW OBC. 

my output requirement is  60 VDC @ 50 Amps

ALSO please let me know how

1. I can run the code is written for TIDM02013 on my custom Power Board, i try to use c2000f280038c mcu as a main controller. 

2. In which file i do modifications as per my hardware to smoothly run the source code.