Other Parts Discussed in Thread: BQSTUDIO, EV2400
Dear all,
I bought the BQ35100EVM-795 EvalBoard but I have had some troubles during its use.
As a matter of fact, once I have prepared the setup as shown on the User Guide SLUUBH7 and connected all to my PC throught EV2400 adapter, I opened "bqStudio" and selected "0100_1_02-bq35100.bqz" file.
However, the application tells that "the detected device is not compatible with this application".
After having pressed the OK button, it shows the main screen but it is clear that the connection is lost.
I am using is a Li-SOCl2 one with a 3.6V open circuit voltage.
I can not figure out how to fix the issue.
Could anyone give me some suggestions?
Thank you in advance.
Kind regards,
Vladimir Zitoli