Hello,
The datasheet for the TPS7A4501-SP states that the device has protection against reverse voltage applied at the output:
"The devices are protected against both reverse input and reverse output voltages. In battery-backup applications where the output can be held up by a backup battery when the input is pulled to ground, the TPS7A4501-SP functions as if it has a diode in series with its output and prevents reverse current flow."
Are there any limitations on how long reverse voltage can be applied?
Thank you