This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100: Wake Up time (GE->HIGH to INITCOMP==1) and activation time (GAUGE_START to GA == 1)

Part Number: BQ35100


Hi,

I am currently trying to do Coulomb accumulation (ACC) with the BQ35100.
I wish to power ON the BQ35100 only when there is current consumption in our application.

I tried to do so with enabling pin GE, however I can notice the time between the command (GE -> HIGH) and the BQ35100 to be fully initialized is about 1.3 seconds.
And then it takes around 700ms for the activation of the command GAUGE_START.

I saw in documentation that registers take 1 second to update and 250 ms for the I2C communication to be fonctionnal so this seems to be the cause of those periods.
I first believed the registers update time was for data measure update as I saw in the datasheet, but it seems to concern all registers.

I am looking for monitoring short events (10ms or less), so this device doesn't seem to fit because we are looking for a period for wake up time + activation time for measure about 1 or 2ms maximum. 
However I am not sure if I am doing the right way.
(I tried by polling read control status, and also with interrupt on ALERT Pin)

And finally I found this topic:
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1130715/bq35100-bq35100?tisearch=e2e-sitesearch&keymatch=BQ35100%25252520INITCOMP#

Can you confirm that the BQ35100 needs such delays to be fully fonctionnal when waking up ?

Does a way to reduce this wake up period exist ?

The firmware version is 1.02, so it seems up to date.

King regards,

Yohann