This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2985: difference between LP2985 and LP2985A

Part Number: LP2985

What is the difference between LP2985 and LP2985A? The datasheet doesn't appear to indicate any differences between the two.

  • Hi SRB,

    The legacy chip version of LP2985 has a VOUT accuracy of ±1.5% typical and ±4% over line/load/temperature range, whereas the legacy chip version of LP2985A has a VOUT accuracy of ±1% typical and ±3.5% over line/load/temperature range

    For the new chip version of both LP2985 and LP2985A, the VOUT accuracy is ±0.5% typical and ±1% over line/load/temperature range.

    Regards,

    Kelsey