Part Number: BQ24192
Other Parts Discussed in Thread: BQ27531-G1, , BQSTUDIO, USB2ANY, EV2400
Hello,
We are using BQ24192 charger with BQ27531-G1 gas gauge. Our gas gauge controls the charger by enabling the GG_CHRGRCTL_ENABLE command. As per the BQ24192 charger datasheet, the charging voltage is 4.208 V (101100).

But in our case BQ studio shows the charging voltage is 4.096 V (100101). Also GG goes in Sleep mode and stops the charging whithout seting the FC to 1. Here REG01 Power-On Configuration Register shows: Charger configuration:, 01 – Charge. P.S we have set the Charging voltage (Configuration -->Charge Termination section) of gas gauge to 4.2 V.
How to change the charge voltage value (4.208 V) of 'REG 04- Charge Voltage Control Register Format' in BQ studio?
Regard,
Janhavi Rane