Hi
For the reference input voltage there is a minimum value of 2.46V and a maximum value of 2.55V stated in the datasheet. On the first page is a initial tolerance of 0.4% stated which is less than the previously stated value. Can you elaborate what is considered for the min and max value that they deviate that much from the initial tolerance of 0.4%?
Thanks in advance for your response!
Kind regards
Lukas